7/15/2010 12:21 PM | |
Joined: 9/6/2008 Last visit: 5/7/2022 Posts: 1121 Rating: (86) |
Hi all well i have created a customized object and i have used the c code that is available in FAQ Entry ID:24193022 , i have compiled the c script and given the tagname as "TAG_NAME" instead of "state" and changed the template picture "TYPCAL_MOT_:MAIN.PDL" as to my configred picture, say for an eg "my_pic.pdl". well my problem is that when i click on the customized object, 1. my pop up screen does not appear. 2. will this code trasfer the tag prefix to my popup window. or where have i gone wrong . it seems that i am lost i have attached the code given in the FAQ. Attachmenttag_prefix.zip (303 Downloads) |
Jazz |
|
7/15/2010 1:22 PM | |
Joined: 9/6/2008 Last visit: 5/7/2022 Posts: 1121 Rating: (86) |
Hi romulus i have run through the OS project editor and i have configured the picture via the picture tree manager. i have given the property name in the "STATE" part. and also i have specifed the popup to be open at that time. i have attached the customized object as a pdl AttachmentPDL.zip (249 Downloads) |
Jazz |
|
7/17/2010 7:48 AM | |
Joined: 9/6/2008 Last visit: 5/7/2022 Posts: 1121 Rating: (86) |
Hi roumulus i changed the script for fixed size and adapted my picture but the tag name is not getting trasfered |
Jazz |
|
7/23/2010 6:53 AM | |
Joined: 9/6/2008 Last visit: 5/7/2022 Posts: 1121 Rating: (86) |
Hi Romulus Sorry for the delay, i was away for a service call. I have attached the script for the same. Attachmentscript.zip (289 Downloads) |
Jazz |
|
Follow us on