7/12/2016 11:00 AM | |
Joined: 5/12/2006 Last visit: 4/18/2024 Posts: 22209 Rating: (2979) |
yes |
7/12/2016 11:05 AM | |
Posts: 57 Rating: (0) |
it is better for me to use the V3 firmware or downgrade it to V2.X? |
7/12/2016 11:08 AM | |
Joined: 5/12/2006 Last visit: 4/18/2024 Posts: 22209 Rating: (2979) |
Hi, you can't downgrade to V2.x if you have a V3 PLC!
Christoph |
7/12/2016 11:14 AM | |
Joined: 8/25/2005 Last visit: 3/21/2024 Posts: 1161 Rating: (110) |
Hello khairul, which Firmwareversion are you using? Operating System Update for SIMATIC S7-1200 CPU Firmware V3 My other idea would be to create a support request and forward your diagnostic buffer entries. |
This contribution was helpful to1 thankful Users |
7/12/2016 11:19 AM | |
Posts: 57 Rating: (0) |
thanks for the info
|
7/13/2016 3:30 AM | |
Posts: 57 Rating: (0) |
my PLC already V3.0.2. is there anymore firmware update for V3?
|
7/18/2016 4:18 AM | |
Posts: 57 Rating: (0) |
all the unit have this problems. what i can do right now, just turn off and run it back. but after 4 days, it happen again. |
Follow us on