5/23/2019 3:10 PM | |
Joined: 3/26/2015 Last visit: 7/9/2024 Posts: 20 Rating: (1) |
Hello, I found the GSDML here: Now you can create a tag table with these addresses (see "TagTable.png"). Since the values are now available as tags, you can connect them in the Energy Suite (see "EnergyObjectTable.png"). For displaying them on the HMI copy the tags from the tag table via drag&drop in your HMI screen (see "HMI.png"). When using the Energy Suite it is also possible to use the Energy Suite visualization Example. Attachmentpng.zip (379 Downloads) |
Last edited by: AutoGen_436301 at: 05/23/2019 15:11:59 |
|
This contribution was helpful to1 thankful Users |
Follow us on