1/30/2016 12:13 AM | |
Posts: 76 Rating: (0) |
Hi all I have a problem with simotion d425 , run is ok but the led of ready is red evertime, the machine was worked and the suddenly, I dont cant information about the fault, the device diagnostic: Event id 16# F364:B284 Also the segment display show 6. and point is flash Attach diagnostic device thanks in advance Attachmentdsaig.txt (644 Downloads) |
2/1/2016 6:16 PM | |
Posts: 76 Rating: (0) |
Thanks for response . Yes I made the device diagnost, and upload now and also the screenshott AttachmentDevice Diagnostics_sim D425.rar (560 Downloads) |
Last edited by: mnada at: 2/1/2016 6:21:56 PM |
|
2/1/2016 6:24 PM | |
Posts: 76 Rating: (0) |
and screnshoot
AttachmentDibujo.rar (444 Downloads) |
Follow us on