6/26/2014 10:06 AM | |
Posts: 2 Rating: (0) |
Dear Support team, SiPass ACC5102 Technical Manual states that RS485 bus connected on ACC5102 controler shall be connected to +5 V wheras POWER is already provided from the ACC5102 LNF interface... Can you explain why we need 5 V? Where can I get the source of 5 V on the ACC5102 ? See page 17 of Technical Manual attached. Many thanks Regards AttachmentSiemens_AC5102_technical manual.pdf (692 Downloads) |
7/18/2014 4:01 PM | |
Posts: 2 Rating: (0) |
It seems to be a close view of the onboard end of line settings switches circuits. Maybe i'm wrong, to be validated. |
Follow us on