12/23/2009 9:19 AM | |
Joined: 4/5/2006 Last visit: 4/24/2024 Posts: 917 Rating: (63) |
Hi C.V. , sorry to post again same previuos question, can you tell what nr is CPU slot and what nr is CP ethernet card slot? In WinCC connection you have to configure CPU slot (not CP) Regard |
12/23/2009 9:23 AM | |
Posts: 10 Rating: (0) |
sorry to post again same answer,
In post 3, i uploaded a picture of the hardware config. The CPU Slot is 4, isn't it? Or i am totally wrong? |
Last edited by: C.V. at: 12/23/2009 9:24 AM |
|
12/23/2009 11:00 AM | |
Joined: 4/5/2006 Last visit: 4/24/2024 Posts: 917 Rating: (63) |
Hi C.V. , usually CPU is in slot nr 2 (check in HW config) parameter you have to set in Industria Ethernet connection are 1) MAC address 2) rack nr (usually "0" if you don't have redundant system, you can check in rack HW configuartion) 3) slot nr. (CPU slot nr in AS HW config) HW configuration in simatic Manager has to be same to HW configuration on installed AS system seems your configuration match correctly and everything should be works if you are using "ethernet connection" in Simatci Protocol Suite Regards |
Last edited by: CBo at: 12/23/2009 11:04 AM |
|
This contribution was helpful to1 thankful Users |
Follow us on