3/2/2011 12:41 PM | |
Posts: 10 Rating: (0) |
Hello |
Last edited by: Assystemes at: 4/9/2011 8:43 AM |
|
3/2/2011 2:42 PM | |
Posts: 10 Rating: (0) |
Thank you for this first approach. Unfortunately I already tried this diagnosis and the two files do not exist in my case .... This morning I changed the system settings of the channel variables using only dialogue "ring formation managed by AS. I no longer use the "transfer if with modifications" because it is an old application and I can not control the use of all the variables .... What bothers me is the crash, it is not possible to activate the task manager, so it is not possible to verify the process SCRIPT. In addition, I valid in the draft, THAT GRAPHICS RUNTIME and TAGLOGGING, the phenomenon also occurs .... It's been three weeks now I lead my research and I think I can now bring down the chart, scripts and even the coating designer ... I believe strongly in the msgbox vbModal, but do not know how to eliminate it. This would allow me to strike a cause of my list .... For the link : http://support.automation.siemens.com/WW/view/en/5669686 I do not know if there might be a relation....
Thank you for your help Cordially G. |
3/2/2011 3:36 PM | |
Posts: 10 Rating: (0) |
It is my client who is behind this project (which dates from 2002?) |
Last edited by: Assystemes at: 3/2/2011 3:38 PM |
|
3/2/2011 4:02 PM | |
Posts: 799 Rating: (42)
|
ok, now I understand... When you followed the "migration document" everything should be ok with your migration, but the "script behaviour" changed while time goes by. So it is possible, that a script which worked well in WinCC V5 will occur errors in WinCC V7. This is not ideal, but I think this can't be impeded when you wan't to advance a product. (But that's just my opinion) I think that maybe the MsgBox is the problem, because as long as the message box appears on the screen (while WinCc is running in runtime mode) it can happen, that the scripts in backround will hang or stop working. You can read this also in the following faq: Why shouldn't you use the Windows MessageBox in WinCC? Can you try to work without the MsgBox in your project? (I think a simple way to replace it is to use a little picture window) regards from Germany |
Follow us on