9/1/2008 5:10 PM | |
Posts: 25 Rating: (2) |
Pls. can you tell us which type of SIMOCODE do you have. Is it the 3UF5 or 3UF7? Best regards |
9/2/2008 9:38 AM | |
Posts: 25 Rating: (2) |
Hello again, You can restore the basic factory default settings on different ways (recommendation see manual page 14-12) 1) over the test/reset button (like in the manual described): - be all parameters moved back on the basic factory default settings - the start-up parameter block is deactivated in the device - the password is deleted in the device. 2) via SIMOCODE ES (as in the manual described): - be all parameters moved back on the basic factory default settings - the start-up parameter block is deactivated in the device - an available password is still in the device - you only can restore the basic factory default settings over command if either no password is available in the device or you have not forgotten the password. The whole SIMOCODE pro manual you found on http://support.automation.siemens.com/WW/view/en/20017780 Best regards AttachmentBasic factory default settings 3UF7[1].pdf (1574 Downloads) |
This contribution was helpful to1 thankful Users |
9/3/2008 2:46 AM | |
Posts: 3 Rating: (0) |
Wow.. it works like a charm!! thanks alot!! |
Follow us on