4/21/2011 3:11 PM | |
Joined: 3/21/2006 Last visit: 4/4/2024 Posts: 10228 Rating: (1181) |
Hello, There have only one way to "get it" - you should order it. Or you can download Step 7 lite version for free: http://support.automation.siemens.com/WW/view/en/34832827 Please read this link: What are the essential differences between Step 7 Lite and Step 7/Step7 professional? Aaa and take a look at step 7 liteThere you will find almost everything concerning the same issue... Best regards, Hristo Mihalev |
Last edited by: UMENCHO at: 4/21/2011 3:13 PM |
|
4/21/2011 8:42 PM | |
Joined: 9/27/2006 Last visit: 4/24/2024 Posts: 12257 Rating: (2665) |
Hello iboulay; You can purchase Step 7 v5.5 and S7-PLCSIM v5.4 as 2 seperate packages: Step 7 V. 5.5: http://support.automation.siemens.com/WW/view/en/43346624 S7-PLCSIM: http://support.automation.siemens.com/WW/view/en/27033164 Or you can purchase the package Step 7 Professional; it allows you to program in all 5 IEC6331-3 languages (by adding S7-SCL and S7-Graph), plus includes S7-PLCSIM. The price of Step 7 Professional would be the same as buying the Step 7 and S7_PLCSIM individually. Getting pricing and purchasing the softwares requires you contacting a local Siemens representative,. The best way to do that is to open the Contacts Worldwide link at the right of this page, andlocate the contacts information for your country. If Siemens operates through a local distributor where you workthey will give you the necessary details. Hope this helps, Daniel Chartier |
Follow us on