1/9/2015 3:59 PM | |
Joined: 5/16/2014 Last visit: 9/12/2022 Posts: 7298 Rating: (2145)
|
Hello baconi, a simple and cheap solution would be the Tool "Copy WinCC Project" from the WinCC Competence Center Mannheim: With the separate external application "Copy WinCC Project" it is possible to copy the complete WinCC project with all databases included. Either you can copy it manually or automatically by calling a WinCC action. The copy is stored in a directory that is chosen by the user. The directory will be expanded automatically by the date of the current day. see: http://www.siemens.de/industrysolutions/de/en/wincc/support/wincc-tools/Pages/Default.aspx Regards Georg Berghof |
PS: If this post did really help you, you may use the Rate-button |
|
Follow us on