11/16/2012 5:34 PM | |
Posts: 510 Rating: (117)
|
Allen1, I am familiar with a CP1434 TCP anda CP2572 for Ethernet communication. Can you confirm the part number you are using? Attached is the CTI manual. There are application examples starting on page 45. Do you need help on the TI side or the 317 side? billwest Attachment2572cti.pdf (520 Downloads) |
Last edited by: billwest at: 11/16/2012 8:50 PMHere is a link on programming the T.... instructions on the S7-300 side. http://support.automation.siemens.com/WW/view/en/29737950 Last edited by: billwest at: 11/16/2012 8:48 PMI found an older version of the manual that had a more extensive example for Send Receive. The TI side would not have to change but you would have to change the AG_Send and AG_RECV to TSEND and TRECV and add a TCON and TDISCON. |
|
This contribution was helpful to1 thankful Users |
11/17/2012 5:36 PM | |
Posts: 54 Rating: (1) |
Thanks for reply, Have you got a example s7 and TI project. I am try communication s7 and TI cp2572. best regards |
11/18/2012 12:45 AM | |
Joined: 9/27/2006 Last visit: 9/19/2024 Posts: 12282 Rating: (2684) |
Hello allen; The following document presents an application example for exchanges between a CP 2572 and a CP 343-1, using an ISO-over-TCP connection. See chapter 2.4 (pages 174/200 and following): SIMATIC 505 Ethernet TCP/IP Communication ...Hope this helps, |
11/18/2012 5:35 PM | |
Posts: 54 Rating: (1) |
Hello dchartier, I dont use cp343-1... thanks for reply |
11/19/2012 12:25 PM | |
Posts: 54 Rating: (1) |
I want s7 and TI cp2572 communication,but not use cp343-1 card.I use s7 integrated profinet port. |
Follow us on