6/24/2020 3:56 PM | |
Joined: 10/10/2005 Last visit: 4/18/2024 Posts: 1917 Rating: (132) |
Hello CharlesChia1986, follow the information from the following FAQ (see link). When migrating the blocks or the STEP 7 program, you already have to consider a lot: https://support.industry.siemens.com/cs/ww/en/view/62100731 With a friendly greeting |
This contribution was helpful to1 thankful Users |
7/3/2020 3:05 AM | |
Joined: 6/3/2020 Last visit: 3/27/2024 Posts: 2 Rating: (0) |
Thank you so much for your information Cicero. May I also ask after downloaded the TIA Portal program into the S7-300 PLC, can I download the Step 7 V5.5 project into the same PLC which is already loaded with TIA Portal Project? Thanks in advanced. |
7/6/2020 2:30 PM | |
Joined: 7/7/2010 Last visit: 4/24/2024 Posts: 14624 Rating: (2348)
|
You can always factory reset the memory card / PLC and load a project, correct?
|
science guy |
|
Follow us on