12/9/2009 4:10 PM | |
Posts: 10 Rating: (5) |
Dear All, You don’t have to archive the project with the Project Scanner but only select the project and the program will move back the project and separate the database. Exit the project scanner and open the project with the error. In my case it solved the problem and I was able to open the project again. |
This contribution was helpful to13 thankful Users |
3/3/2010 6:59 PM | |
Posts: 134 Rating: (11) |
good solution, works fine. I wonder if detaching wincc database would do the same thing?
|
This contribution was helpful to1 thankful Users |
3/27/2014 1:25 PM | |
Posts: 86 Rating: (7) |
Hello, I faced the same problems, with the same versions. Is there someone who solved this? Thanks. Yer |
3/27/2014 2:52 PM | |
Posts: 86 Rating: (7) |
Thanks to Silent Bod I solved the problem! /tf/WW/en/Posts/79008#top Thanks, Yer |
This contribution was helpful to1 thankful Users |
3/27/2014 4:02 PM | |
Posts: 134 Rating: (11) |
There are lots of tips in his post, what tip solved your problem? |
Follow us on