11/20/2019 11:28 PM | |
Posts: 9 Rating: (0) |
[snip] As an aside, and this is probably better in a different thread, I am trying to add a driver for an mPCIe cellular modem which requires editing of the OS source code and rebuild. I have been given a Make file from the manufacturer to do this, but I am still unsure after reading this forum of the process to do this? Do I run the Make process over the source code generated by the previous build process (using kas) and then rebuild? Which directory does the source for rebuilding live in? Or am I better off creating a new recipe from the Make file and adding it before re-running the kas build? Can you recommend a good tutorial on how I would go about this process. Thanks ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/02/2019 12:19:21New subject after splitting. Division of questions into seperate topics. |
|
11/24/2019 10:26 PM | |
Posts: 9 Rating: (0) |
I have not applied any changes to the Zeus dependent layer, as I have not been able to get it build. My thinking was to run the KAS build process like in the manual, make the changes to the source code generated by the KAS process, then re-compile. But I don't think this is correct. Documentation for the modem driver is attached, specifically section 3.2. The manufacturer's support has supplied me with a Make file to apply these changes once I have access to the source, which I have been able to apply as above. I have asked the question and they do not have any BitBake layers or recipes that would make this process easier. Thanks for your help AttachmentQuectel_WCDMA<E_Linux_USB_Driver_User_Guide_V1.9_Preliminary_20190325.pdf (209 Downloads) |
12/9/2019 8:18 AM | |
Joined: 4/28/2015 Last visit: 6/28/2024 Posts: 578 Rating: (43) |
Go to network settings. If that detects a modem, it will present it besides eth0 / eth1 as interface. |
1/24/2020 12:57 AM | |
Posts: 1 Rating: (0) |
Did you manage to get this working at all I am just embarking on the same journey!!! |
Follow us on