11/17/2019 9:07 PM | |
Joined: 3/25/2019 Last visit: 2/20/2024 Posts: 4 Rating: (0) |
Hello. I use TRCV_C and TSEND_C to communicate between 1214C CPUs (V4.2) without any problems. I wish to communicate between PLCs using TRCV_C and TSEND_C by the CP1243-1 (6GK7243-1BX30-0XE0 V3.1.40), but I can't make it work. I attach a picture of an sample project that works well, I also attach a picture with the same project but with a link between the two CP1243-1, but this don't work. Can someone help me?
AttachmentSample and pictures.zip (64 Downloads) |
Follow us on