10/10/2012 3:34 PM | |
Posts: 29 Rating: (0) |
Hello Experts.
To do's: I'm a lazy and I'm trying to do a template that I want to reuse in every project that I'll have to implement. For that I'll try to implement in WinCC some better view WinCC flex faceplate, where I set only the tags, and all the internal connections are automatically realised. Realization of target: Till now I createa a nice command windows 7 aero look-alike, with the following tabs:General, Additional information, Alarms, Graphics. The command windows is the file: blower_command_window. This tab command windows appears when I press motor M1( M1 is the one on the left in the example) . The VB code for this is: Dim picWindow: Set picWindow = HMIRuntime.ActiveScreen.ScreenItems("Picture Window1") picWindow.PictureName = "TABTest.PDL" End Sub Tab switching is realised as I'll describe in the following lines. On the picture windows that I've putted on the main screen, I've putted 4 button on the top of the PDL. On each button, I've select a new PDL, and Deactivate the active button. The code is for example: ScreenItems("TAB").PictureName = "TAB2.PDL" The conclusion, I have 4 pdl, in a pictures window, that is inside a picture windows. For a better understanding please look at the pictures attached.
Thank you in advance, for any suggestion. AttachmentF:\SCREENS.zip (85 Downloads) |
Follow us on