11/29/2011 2:13 PM | |
Joined: 9/29/2005 Last visit: 4/26/2022 Posts: 313 Rating: (24) |
Hi Ben... you are right. That´s the same reasonwhy this CP is not able to reach any other ethernet device through the CP-CPU-interface. It will be supported with a CP and CPU FW-update but not before the end of 2012. Alternatively you have to use a device like the SINAUT MD741-1 EGPRS-ROUTER or SCALANCE M873-0 UMTS-ROUTER. However when you have a IP-connection (with corresponding settings inmodem/router/firewall...) or even a VPN-connectionyou can have a automatic download of the logfile without webserver: One possibility for downloading the files can be done by the Mozilla Firefox download-mechanism - you can download a file by using the following pattern: [Path to Firefox.exe] [Path to file on webserver] e.g. "C:\Program Files\Mozilla Firefox\firefox.exe" "https://192.168.0.1/DataLog.html?FileName=TankStat.csv" This line can be inserted in a batchfile (e.g. "CollectDataLogs.bat") and this batchfile can then be called e.g. by the Microsoft scheduler regularly. You can also add more lines to this batchfile to get several datalogs from different CPUs. Another option would be a downloadmanager (e.g. Orbit Downloader), where you enter the download address (e.g. https://192.168.0.1/DataLog.html?FileName=TankStat.csv) and let the downloadmanager download it regularly. well i hope this will work with the M873. I only read the technical data... |
7/30/2014 2:58 PM | |
Joined: 5/29/2013 Last visit: 5/2/2024 Posts: 100 Rating: (28) |
is it already possible ? We are now already in 2014
|
Regards |
|
10/8/2015 4:48 PM | |
Posts: 2 Rating: (0) |
I would also be interested in. Dose some body know the answer yet? |
Follow us on