7/2/2013 2:51 PM | ||||
Posts: 4 Rating: (0) |
Hi I have downloaded the Program exampel "Web Server"
I installed it on a 6ES7 214-1AG31-0XB0 Firmware V 3.0.2 I can see the Number changing in the browser so fare so good, but when i want to Change state of a bit or change a Integer nothing happensI have used Google Chrome and IE10 as Browser. Any good ideas??
|
|||
7/2/2013 3:18 PM | ||||
Joined: 7/7/2010 Last visit: 9/20/2024 Posts: 15212 Rating: (2417)
|
Did you login to the default web server page before starting your user defined pages? |
|||
science guy |
||||
7/3/2013 7:36 AM | |
Posts: 4 Rating: (0) |
Yes i typed in the IP adress on the CPU and then clcik the user defined web page, Everyting works fine execpt from changing bit and Values in the PLC. |
7/3/2013 8:21 AM | |
Posts: 461 Rating: (29) |
huggy_d1 told about login not simply accesing the user defined pages from browser.. Login only allows u to make changes from browser to plc ....With out login u can simply monitor the values in ur browser Regards, Nelliyan.G |
Last edited by: Nelliyan randy at: 7/3/2013 8:21 AM |
|
7/5/2013 12:18 AM | |
Posts: 98 Rating: (6) |
Hey, They're right; did you already login as "admin"? On the left side of the standar page you have to sign admin and then click log in. Attached there's the info about log in or look on the Manual of s7-1200 AttachmentSIMATIC S7 S7-1200 Programmable controller - Layout of the standard Web pages.pdf (233 Downloads) |
7/5/2013 8:26 AM | |
Posts: 4 Rating: (0) |
Thanks have a nice Weekend |
Follow us on