3/21/2019 9:37 PM | |
Posts: 1 Rating: (0) |
hello, PLC: 1214C AC/DC/RLY TIA Portal: v14 SP1 I try a lot of hours and I can't solve my problem. I create webserver and datalog and this working but I would like to create a new file with new name per month. But my program generates only for two months. First when I download the program to CPU and second when M44.0 is first an activating edge. Next edge marker M44.0 doesn't generate a new file on the webserver. Can you help me? What I do wrong? Below I join screen my program.
AttachmentMyProgram_WebServer.pdf (200 Downloads) |
Last edited by: unknow123#wewe at: 3/21/2019 9:46:58 PM |
|
3/23/2019 4:10 AM | |
Joined: 10/27/2017 Last visit: 9/14/2024 Posts: 59 Rating: (0) |
Hello. You can use Memory Card to increase the load memory, the size of the memory will then depend on the Memory Card |
Follow us on