5/30/2010 10:07 AM | |
Joined: 8/22/2009 Last visit: 7/11/2024 Posts: 42 Rating: (1) |
What are the limitations of using modbus tcp wizard (Demo version)? |
Veolia |
|
5/30/2010 1:52 PM | ||
Joined: 9/27/2006 Last visit: 9/19/2024 Posts: 12282 Rating: (2684) |
Hekko Ahmed; The Modbus TCP wizard, to my knowledge, is always in demo mode.There is no license to purchase for the wizard. It is a piece of software that you downkoad for free, that uses the,Net platform (that is installed with Step 7) and that generates a DB containing the self-generated parameters that the Modbus TCP package can use as reference in your project. http://support.automation.siemens.com/WW/view/en/31535566 If you have purchased and installed the Modbus TCP package (product number: 2XV0 450-1MB02) as seen here, in the various downloadable files, then whatever the wizard has generated can be used in your project. http://support.automation.siemens.com/WW/view/en/22660304 Hope this helps, Daniel Chartier |
|
Follow us on