5/6/2020 12:47 PM | |
Posts: 18 Rating: (0) |
[snip] My new problem: For example, I would like that when I press the button 1 on my web page, the elevator goes to floor 1. I don't know what I should put on my inputs so that when I click on it, it activates the project. Thanks you ! ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/06/2020 13:08:21Edited text for better reading. Last edited by: Jen_Moderator at: 05/06/2020 13:10:29New subject after splitting. Division of questions into separate topics. |
|
5/6/2020 2:57 PM | |
Posts: 18 Rating: (0) |
It is not possible to do both at the same time ? I would like to make it work with the buttons on the control box and with the remote web server |
5/6/2020 3:46 PM | |
Posts: 18 Rating: (0) |
OK Watch my picture. If I do as in the example above my program normally it should work both ways? ( Whith the control box and with the web serveur ) Thanks |
5/6/2020 4:12 PM | |
Posts: 18 Rating: (0) |
Yes i know thats is not good but if i add a a network input and a input bloc with OR that's good ? |
Follow us on