1/24/2016 7:06 PM | |
Joined: 5/9/2015 Last visit: 9/5/2024 Posts: 81 Rating: (4) |
Dear Georg, Thanks for your response. Can you please suggest some document from where i can check which license is required for wincc single station reference application. In my project i have one Wincc single station and one wincc single station reference application. While downloading the project from ES, i am successfully able to download the project without any error. but when i activate the runtime on the referecne application machine, the project get deactivated automatically and gives two error messages as attached. 1. Unspecified error 2. No Runtimeproject found. Then I have unchecked the “Alarm logging runtime” and “Tag Logging Runtime” from the startup list and able to activate the runtime but there is no trend and alarm is coming on this station. Please suggest what could be the reason fro that. Presently i am on project site, a quick response will be highly appreciated. Thanks in advance Best regards, Naresh Saini ------------------------------------------------------------------------------------------ Attachmenterror message.zip (536 Downloads) |
Last edited by: nkr at: 1/24/2016 7:57:31 PMLast edited by: Min_Moderator at: 1/25/2016 2:21:56 PMNew subject after splitting |
|
9/14/2018 9:32 AM | |
Joined: 8/5/2014 Last visit: 9/5/2024 Posts: 164 Rating: (6) |
Any suggestions ? Best regards, |
Regards, |
|
Follow us on