12/12/2018 6:05 AM | |
Posts: 5 Rating: (0) |
Hi guys! We have in our plant these Robicon GENIV GH 180 drives which have not been running for the past 12 months as we had shut down production in that period. Now that we are close to resuming production, I understand that we will need, among other things to reform the DC-bus capacitors. The last time this was done is back in 2016 during plant commissioning, so I remember quite a little of how to do it precisely. I'm wondering if you can help me with a step-by-step guide on how to proceed. We have a 0-450V variac which I am well conversant of how to use; it's the details of where exactly to connect on the drive and mode/parameter settings which I am not familiar with. I attach the drawing showing the secondary terminals of the transformer so that you can say if possible, where exactly should the output of the variac be connected. Thanks! ------------------------------------------------------------------------------------------ AttachmentConverter wiring diagram.pdf (585 Downloads) |
Last edited by: Jen_Moderator at: 12/12/2018 12:24:37 PMNew subject after splitting |
|
12/12/2018 1:07 PM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
Closed cause question posted twice. The second thread with the subject Reforming of DC-Bus Capacitors is published within the conference ROBICON Perfect Harmony - Medium voltage converters.
Jen_Moderator |
Follow us on