10/22/2019 2:57 PM | |
Joined: 9/30/2016 Last visit: 4/5/2024 Posts: 910 Rating: (6) |
Please also see the attached screenshots. I am trying to update a WinCC server from WinCC 7.0 (running under Windows 7 Enterprise) to WinCC 7.4 (running under Windows Server 2012). My Engineering Station is has WinCC 7.4 running under Windows 10 in a VM-ware machine running under Windows 10. I have downloaded the project from VersionDog (our backup program) to the Engineering Station and accepted that the project is migrated from WinCC 7.0 to WinCC 7.4. I have installed WinCC on the server running Windows Server 2012 and now I need to download the project from the Engineering station to the Server. I have modified the ip addresses of both the server and the Engineering station to be as they should be in the real world - and I have also set the user on the ES to be the same as the user on the server. The 2 computers are connected to a simple (unmanned) switch and they can ping each other. The can also see each other in Simatic shell. I can start the (full) download and it SEEMS that the whole project is copied to the WinCC server but the ES freezes with the message "opening the project". After I kill the WinCC task on the ES I cannot do much with the project until I stop (and restart) WinCC SQL service. But even after this the project on the server cannot be opened - I get a error massage saying that the Windows rights are insufficient. If I delete the project on the server (only possible after stopping the service as mentioned) and manually copy it in via a USB disk I also get the error massage about the missing Windows right. What am I doing wrong and how can I fix it? AttachmentDownload of full project.zip (36 Downloads) |
Follow us on