5/19/2020 8:02 AM | |
Joined: 9/30/2016 Last visit: 4/5/2024 Posts: 910 Rating: (6) |
Please also see the attached screenshots. I am modifying a FB and need to add some static variables to the interface. When I save the FB I am told that there are no parameters and local variable names available due to a time stamp conflict (see the screenshot). Will this sort it self out when I download the FB to the PLC - or what do I need to do? AttachmentFD1 Vikler alarms A.zip (79 Downloads) |
Follow us on