1/4/2012 10:24 AM | |
Posts: 1776 Rating: (95)
|
Hi, how is your procedure? Can you open the source project with V7.0 SP1? Do you run the duplicated project on the same computer? |
1/4/2012 10:56 AM | |
Joined: 4/19/2011 Last visit: 5/10/2024 Posts: 18 Rating: (0) |
Hai , Existing winCC 7.0 sp1 project does not work , we tried to duplicate could not duplicate ! I can attach the diagnose folder , is there any suggestion to solve this problem ? Regards, Attachmentdiagnose.zip (125 Downloads) |
1/5/2012 11:47 AM | |
Posts: 1776 Rating: (95)
|
Hi, maybe your system is corrupted. See the diagnostic file PMDiagnose.log. At the end of the file you can see that you cannot access to the .mdf (configuration database) file. This means you have no permission or your .mdf is corrupted. You have this porblem since 2011_11_29 11 11:56:59:390 CCProjectMgr.exe CSingletonProject::AttachDatabases pICCDBManagement->AttachDatabase \\STEER\WinCC_Project_oa-324_hmi\oa-324_hmi.mdf on STEER failed: 0x80040000 So take a saved project before this date. btw see also the link http://www.votedemos.com/0x80040000.php |
Follow us on