8/12/2013 8:10 AM | |
Posts: 16 Rating: (1) |
Generally encountered such a problem that sometimes seems to hang at the enterprise WinCC. The logs have the following (excerpt)WinCC_Sys_01.log,SCRIPT.log,PMDiagnose.log There is a program halt script WINCC + off the computer: [code] int RetMsg; RetMsg = MessageBox (NULL, "Вы действительно хотите закрыть программу и выключить компьютер?", "Системное сообщение", MB_SYSTEMMODAL | MB_OKCANCEL ); if (RetMsg == IDOK) { SetTagBit("Start_Stop",FALSE);//Turn off the unit DMExitWinCCEx (DM_SDMODE_POWEROFF); } [/code] Is it possible that the function DMExitWinCCEx - Trouble is this? And help, if you set this function flag - DM_SDMODE_FORCE_POWEROFF? AttachmentLogs.zip (157 Downloads) |
Last edited by: W1nn1ep00h at: 8/12/2013 8:44 AMLast edited by: W1nn1ep00h at: 8/12/2013 8:14 AMLast edited by: W1nn1ep00h at: 8/12/2013 8:14 AM |
|
8/12/2013 1:19 PM | |
Posts: 1530 Rating: (59)
|
Hello W1nn1ep00h, did you take a look at readme of your WinCC-Version? There you will find this: 2.2.1 Deactivation and shutdown of a redundant PC via ODK functions To avoid the display of the dialog "SIMATIC WinCC Redundancy" when deactivating or shutting down a redundant server, instead of the ODK functions "DMExitWinCCEx" and "DMDeactivateRTProject", use the following functions: - Deactivate the WinCC project: "DMDeactivateRTProjectEx" with the parameter "DM_DEACTIVATE_FORCE" - Close the WinCC project and shut down the PC: "DMExitWinCCEx" with the parameter "DM_SDMODE_FORCE_POWEROFF" |
Last edited by: Bizur at: 8/12/2013 1:21 PM |
|
This contribution was helpful to2 thankful Users |
8/12/2013 1:39 PM | |
Posts: 16 Rating: (1) |
Thank you for the tip. The very old document found in German with this description - here
|
Last edited by: W1nn1ep00h at: 8/12/2013 1:40 PM |
|
Follow us on