10/11/2016 4:22 PM | |
Joined: 11/14/2008 Last visit: 5/6/2024 Posts: 504 Rating: (22) |
Maybe this is fixed in the latest updates ? Have you already checked release notes ? Latest version of TIA V13 is TIA v13 SP 1 Update 9 Updates for STEP 7 V13 SP1 and WinCC V13 SP1 |
10/12/2016 8:37 AM | |
Joined: 11/14/2008 Last visit: 5/6/2024 Posts: 504 Rating: (22) |
sorry for being strange :D , Yes I saw TIA Portal and send that, sorry for that but which exact version of Wincc 7.3 do you have ? I checked release notes of the updates for Wincc 7.3 and there are some improvements for these type of connection (although PLC sim is not mentionned they do mention S7-1500 and it's protocol...) may be worth to check :) Update 8 for WinCC V7.3 and WinCC V7.3 ASIAHope it helps, Regards, |
Follow us on