1/11/2021 5:47 PM | |
Posts: 2 Rating: (0) |
Hi, I have installed WinCC 7.4 SP1 Update 11 in Server System(Windows Server 2019 Standard) and trying to connect it to S7-1500 PLC. But am facing communication issues. I have checked the common suggestions that i got in the forum as follows: * I have installed Simatic Net V15 SP1 *I have checked TCP/IP, Siemens Communication Settings and In Driver settings for Port name and Address. Everything Looks fine. *I do not have any password protection in my PLC or SCADA. I had an error while installing the SIMATIC NET Software saying "The following program could not be installed: SIMATIC NET PC Software V15+SP1 Setup cannot complete the installation". After this i tried installing Simatic Net again, and this time it was installed successfully without any errors. But the Communication issue was not solved. Then i formatted the server and reinstalled all the software, But again i got the same error as before while installing the Simatic Net software. i tried again to install simatic net software and it was installed without any error. But the Communication issue was not solved. I have attached the Log file for reference. ------------------------------------------------------------------------------------------ AttachmentSIMATIC_S7-1200__S7-1500_Channel_01.txt (91 Downloads) |
Last edited by: Jen_Moderator at: 01/12/2021 09:24:52New subject after splitting |
|
1/12/2021 9:43 AM | |
Joined: 8/12/2020 Last visit: 7/15/2024 Posts: 41 Rating: (3) |
Hi SudeepKelaginame, The use of WinCC 7.4 SP1 on Windows Server 2019 Standard is not released by Siemens. On the other hand, the use of Simatic NET 15 SP1 with WinCC 7.4 SP1 is also not released by Siemens. These incompatibilities may be causing the problems you mention. You can check the compatibility of Siemens products throught the Compatibility tool. BR, |
Last edited by: Hugens at: 01/12/2021 09:56:56 |
|
Follow us on