11/10/2020 2:44 PM | |
Joined: 5/16/2014 Last visit: 9/12/2022 Posts: 7298 Rating: (2145)
|
Hello ThaKibosh, the database 'CC_ExternalBrowsing' has a similar catalog-function You should have a look to the Application example: https://support.industry.siemens.com/cs/ww/en/view/38132261 Regards Georg Berghof |
PS: If this post did really help you, you may use the Rate-button |
|
12/4/2020 11:45 AM | |
Joined: 5/31/2011 Last visit: 4/24/2024 Posts: 190 Rating: (31) |
I have to correct you about the "CC_External_Browsing". You can also access the actual runtime data without configuring any back-up archives. To activate "CC_External_Browsing" just open "WinCC Archive Connector" without making any configuration. Just leave everything empty. In the tab "Connect/Disconnect Archive" just click "Connect". Now "CC_external_Browsing" magically appears as a database in SQL and you can read out tag-logging and alarm-loggings with the WinCC OLEDB Provider. Now I'm still looking to access the "User Archives" without having to connect to the runtime database. |
Last edited by: ThaKibosh at: 12/04/2020 11:46:19 |
|
This contribution was helpful to1 thankful Users |
12/4/2020 1:44 PM | |
Joined: 5/16/2014 Last visit: 9/12/2022 Posts: 7298 Rating: (2145)
|
Hallo ThaKibosh, the Userarchives are only simple tables in the See Manual "WinCC/Connectivity Pack V7.5" https://support.industry.siemens.com/cs/ww/en/view/109760723/39106454027 Mit freundlichen Grüßen Georg Berghof |
PS: If this post did really help you, you may use the Rate-button |
|
Follow us on