5/21/2007 12:11 PM | |||||||||||||||||||||
Posts: 28 Rating: (1) |
Dear all, I met a strange phenomena about the license. In one project, the system is PCS7 V6.0SP3, server/client struct, redundency server, muti-client. The licenses installed for server: 1.Simatic WinCC Server 2.Simatic WinCC-V6 RT 100KPTg 512 ATg 3.Simatic NET BCE/Windows 2000 4.Simatic SFC Visualization V6.0 5.Simatic WinCC Reduncancy 6.Simatic WinCC Advanced Process Ctrl The licenses installed for client: 1.Simatic Wincc-V6RT 128PTg 512 ATg. When rnning, no alarm from server, But there is always POP displayed in client, which contnet is: Wincc Authorizations are not installed or are insufficient
Additional information Can be found in the following file C:\Program Files\SIEMENS\WINCC\Diagnose Attached is the diagnose file. P.S. the client only running time, no any wincc explore opened. Please help me. Thanks! AttachmentAuthorinformation.zip (220 Downloads) |
||||||||||||||||||||
5/22/2007 5:11 AM | |
Posts: 28 Rating: (1) |
Hi, Danielle, Nemo Attached please find the installed license keys in server and client. The licenses checked ok. And no defragmentation done in PCs. The c/s struct is copied from the siemens standard. By the way, the server and all clients runing normally,except thepop-up windowin client. And you can push "OK" or "CANCEL" for the window to close it, nothing else happens. For the files in WinCC/diagnose, I am contacting the site. I will attach later. Thanks! Attachmentlicense.zip (239 Downloads) |
Last edited by: debon at: 22.05.2007 05:15 |
|
5/22/2007 8:51 AM | |
Posts: 1084 Rating: (72)
|
Hi, I see that you installed the licenses on the "G"-drive Did you install wincc on the "G" drive aswell? with regards, Ikkezelf |
5/22/2007 9:06 AM | |
Posts: 28 Rating: (1) |
hi, Ikkezelf, The last attachment are just an example to show the detailed license info. In the site pc, the SW and the license are both installed in C disk. BR. |
Follow us on