4/30/2020 8:38 AM | |
Joined: 8/3/2009 Last visit: 9/20/2024 Posts: 13753 Rating: (1735)
|
Hello dstudio If your Project is in WinCC flexible 2008 Sp5 then download the SP5 from and install it: https://support.industry.siemens.com/cs/ww/en/view/100777999 Its also released with Win7. -> I Would also reccomend installing the Upd2 on the Engineernig System and on the Runtime System. Then compile and load the Project again. https://support.industry.siemens.com/cs/ww/en/view/109757233 Dont forget to set the PGPC INterface to the right accesspoint and Communication adapter or Networkcard Combination. Bye Murof |
If this Information really helps, you could use the Rate function |
|
5/3/2020 8:58 AM | |
Joined: 8/24/2006 Last visit: 5/31/2024 Posts: 148 Rating: (9) |
Hello, upodate not works, please have a look to attachment. I download more times, with different pc..same issue |
5/13/2020 11:34 AM | |
Joined: 8/24/2006 Last visit: 5/31/2024 Posts: 148 Rating: (9) |
Hi, thank you. I download and tried more of one time: no success. So I reject. Thank you again |
Follow us on