5/22/2020 11:06 PM | |
Joined: 4/13/2010 Last visit: 4/9/2024 Posts: 2 Rating: (0) |
Good afternoon, When I try to download to a TP177B HMI or any other HMI, then the Runtime Error! See the attached screen image. The error message has the following message: - Microsoft Visual C ++ Runtime Library. When I compile there is no error, it is only when I try to download it and after the PG communicates with the HMI then this error occurs. Would you help me?
Attachmenterro doc.doc (150 Downloads) |
5/28/2020 12:14 PM | |
Joined: 8/3/2009 Last visit: 4/25/2024 Posts: 12869 Rating: (1640)
|
Hello Evandrovs I would try this: https://support.industry.siemens.com/cs/ww/en/view/36645252 and if it does not help, then try a reinstall of WInCC flexible. I looks like some component is missing or damaged. Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on