1/7/2021 11:52 AM | |
Joined: 10/19/2017 Last visit: 4/16/2024 Posts: 49 Rating: (0) |
Hi All, WinCC version 7.5 SP1 Upd4 I've installed the client, BPC and APC. I have a problem with WinCC webnavigator I did the following steps: - Server package created - Published pictures (Client only "@pictures" and with server prefix all pictures) - Published scripting (Client only, not with server prefix) When I start the webclient it looks good. But when I try to open pop-up it shows "failed to load http://<servername>/<serverprefix>__\<folder>\<picturename.PD_> Where <serverprefix> is the prefix you fill in when the pictures are being published. What I find strange is the extra "__\" between serverprefix and folder. If I look at the published pictures in the webnavigator it shows this: <serverprefix><folder>\<picturename.PD_> Does someone know where the extra "__\" comes from? I've added some pictures. AttachmentFailedToLoad.zip (196 Downloads) |
"To the optimist, the glass is half full. To the pessimist, the glass is half empty. To the engineer, the glass is twice as big as it needs to be." |
|
1/8/2021 8:01 AM | |
Joined: 5/16/2014 Last visit: 9/12/2022 Posts: 7298 Rating: (2145)
|
Hello Tinuz, you are using Basic Process Control in the Basic-Runtime-Project see manual "SIMATIC HMI WinCC V7.5 SP1 WinCC Information System" https://support.industry.siemens.com/cs/ww/en/view/109772961/88058181387
Georg Berghof |
PS: If this post did really help you, you may use the Rate-button |
|
Follow us on