4/27/2016 12:13 AM | |
Joined: 5/28/2008 Last visit: 9/21/2024 Posts: 4515 Rating: (839) |
Hello, Hope the following link will help. What remedies are there when you can't load the configuration of the PC station? |
Ayman Elotaify |
|
4/27/2016 2:15 AM | |
Joined: 11/17/2014 Last visit: 8/28/2023 Posts: 184 Rating: (0) |
Thanks Ayman, I'll check it out now |
4/27/2016 8:28 AM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating: (1181) |
https://support.industry.siemens.com/cs/ww/en/view/21914005 |
4/27/2016 9:00 AM | |
Posts: 107 Rating: (20) |
If you need to configure H-System (PCS7) with your station using PLCSIM, Named Connection protocol (wincc generated tags) can't be supported, So you need to add S7-Connection instead of S7-Connection fault-tolerant. During Compilation, the tags will be generated under TCP/IP instead of Named connection. I have attached screenshots for more understanding AttachmentWINCC PLCSIM.zip (224 Downloads) |
This contribution was helpful to1 thankful Users |
4/29/2016 1:26 AM | |
Joined: 11/17/2014 Last visit: 8/28/2023 Posts: 184 Rating: (0) |
Thanks a lot guys, I'll try and then update you. I appreciate. |
Follow us on