10/28/2014 5:33 AM | |
Posts: 42 Rating: (3) |
Hi all, I know it is a little bit late to ask this question. I am doing a system migration project as mentioned above. I understand that WinCC 5.0 SP2 can migrate to WinCC 6.2 SP3 then from there to 7.. I have done the installation for WinCC 6.2 SP3 by following the manual as attached. I got the error message from diagnostic file "CCMigrator.txt" as below, "Error While opening WinCC project. hr = 0x80046211. CS AlarmLogging could not be updated." "Migration finished with errors" From the forum, I found similar issue from other user, solved by reset the archives from Alarm Logging. But I can't find this "Reset" function is WinCC 5.0 version. Then I try to create a new project in WinCC 5.0, and I transfer only the graphics to the new created project. and try to do the migration again. Unfortunately, I got the same error again. I just can't understand why is this happen to a new created project without any Alarmlogging configuration. *The attached migration manual is showing WinCC5.1 to version 6, and I assume WinCC 5.0 Sp2 can do the same way. Can anyone teach me what to do from now? Thank you and have a pleasant day! Sytupit
AttachmentWinCC_Upgrade_V4_To_V7_en.pdf (506 Downloads) |
Last edited by: Sytupit at: 10/28/2014 5:38 AM |
|
10/28/2014 3:12 PM | |
Posts: 42 Rating: (3) |
Hi Georg, I managed to get a WinCC6.0 SP3 installation CD, and the issue didn't appear on this migration. So much thanks for your help. But then i got another error message as attached. There are 4 graphic pages got error, "While saving, invalid object references were found in the picture....". I tried to open the project in WinCC 6.0 and I can see these 4 graphic pages appear in "Graphics Designer". Should I fix this issue and do a migration again (with V5.0 backup copy) until I see the words "Data migrated successfully" or I can proceed to the next step by using this project file? Would it be something didn't get migrated due to these errors and the migration aborted? Thank you and have a pleasant day! Sytupit
AttachmentConvert.zip (226 Downloads) |
Follow us on