11/19/2008 8:08 AM | |
Posts: 75 Rating: (0) |
Old project: New project station Scenic (WinCC V4) with CP5412 (address 2) replaced on Rack PC IL40 (WinCC6Sp4, CP5614A2) - used xdb on Station Configurator station Scenic (WinCC V4) with CP5412 (address 1) replaced on Rack PC IL43 (WinCC6Sp4, CP5613A2) - used xdb on Station Configurator CP5431 don't programmed.
Rack PC IL43 (WinCC6Sp4, CP5613A2) connect to CPU317-2 - no errors, connect to S5 controllers don't work! (255,13.11.2008,10:39:07:437,1000200,4,,C27_2,DataManager Runtime,Unit 0 of CommunicationDriver "PROFIBUS FMS" cannot be started for run time, dwError1 = 1c253b8, dwError2 = 24b, dwError3 = 1b16f08 Error during initialization of the FMS hardware CP5412/A2.) Bus nodes from console active - 1,2,3,4,10 Why connect to S5 controllers from station don't work? AttachmentRack PC IL 43.zip (55 Downloads) |
11/20/2008 6:59 PM | |
Posts: 75 Rating: (0) |
Hi *Manfred* Project WinCC on station Rack PC IL43from Rack PC IL40 (WinCC6Sp4, CP5614A2 connect to two controllers S5-115U on Profibus channel - no errors,and CPU317-2 - no errors) Best Regards Dimbas |
11/21/2008 8:32 AM | |
Joined: 5/28/2008 Last visit: 12/8/2015 Posts: 901 Rating: (136) |
Hello Dimbas, please contact the Siemens technical support and tell this problem... sorry |
Follow us on