11/4/2017 8:02 PM | |
Posts: 12 Rating: (0) |
Hi nulizhang I have a tool changer in a CNC machine that is works by the PLC Omron and Drive Omron which work by pulse / direction Output 24v from PLC, and this Drive was damaged, I need to replace it with the SIMODRIVE 611U 6SN118-1NK01-0AA1 and servo motor 1FK7022-5AK71-1TG3-Z. I'm trying to use Angular incremental encoder interface as input. |
11/8/2017 7:26 AM | |
Joined: 10/17/2007 Last visit: 5/4/2024 Posts: 3981 Rating: (340) |
Try to use 611U encoder feed back card--6SN1118-1NHxx-0AAX and servo motor with encoder easily making 611U in position control --rotary axis
|
If you like my comments please |
|
8/7/2018 8:10 AM | |
Posts: 12 Rating: (0) |
But knowledge and learning are more expensive than time and money I'd better learn how to do it. Thank you. |
Follow us on