8/15/2018 11:48 AM | |
Joined: 3/14/2008 Last visit: 3/29/2024 Posts: 2059 Rating: (924)
|
Can you do a test for me? Open apdiag.exe (...SIEMENS/WinCC/utools) folder and open the output window. Open a SFC and post back the results in the output window (if there are any). |
If I could help you, you can use the RATE button. Thank you. |
|
8/17/2018 8:38 AM | |
Posts: 3 Rating: (0) |
Thanx for your response. Whenever I am clicking to any SFC icon to open the SFC in the Operating Station the whole system getting hanged for few minutes. the apidiagnose screen which is changing time to time is attached to thius message. Please have a look and advice me the needful.
AttachmentIMG_20180817_114733.pdf (94 Downloads) |
8/17/2018 12:19 PM | |
Joined: 3/14/2008 Last visit: 3/29/2024 Posts: 2059 Rating: (924)
|
Hi, In picture: "SGP_WATERCIRC_E" is an object: "StaticText126" and under attribute: "Text" in that object is a wrong tag is linked, one that does not exist. It could be very possible that it completely hangs C-script. Remove or change the tag and I think it should be OK |
If I could help you, you can use the RATE button. Thank you. |
|
8/18/2018 9:01 AM | |
Posts: 3 Rating: (0) |
Dear Oreca, this is not the problem with tag. Actually whenever the SFC button is clicked on the screen it is taking 15 to 20 minutes to be visible on the SFC window as shown in the attached Word Document (Image1 is just after clicking the SFC button, and Image2 is after 20 minutes of time after clicking when its just opened properly) . During this 15 to 20 minutes of time if anyone tries to operate a different operation in the same Operating station , the screen got hanged until the SFC is visible into the SFC window which is not acceptable to the client as it is creating problem in the normal operating proceudre. Please Help AttachmentSFC_Problem.docx (71 Downloads) |
8/20/2018 9:13 AM | |
Joined: 3/14/2008 Last visit: 3/29/2024 Posts: 2059 Rating: (924)
|
Hi Subhorse, Ahh, I understand what you mean. The faceplate is loading, but the SFC section does not load until +/-20 minutes have passed.. That is weird. SFC Visualization is based on ActiveX controls...Maybe there is a problem with your Windows or can be related to a bad install of PCS7. Can you give me some more info: - Which operating system/build/servicepack/64 or 32 bits - Did it work before properly or didn't it work from the start after install of PCS7? - Did you install the PCS7 package option or did you select separate options during install of PCS7. During install PCS7 provides options to install a Engineering Station or Single Server station or …. - You can also upload xml from the Siemens Installed Software, you can reach it from Start->SIEMENS folder. - Does your even viewer show any errors or faults which could relate to PCS7 or ActiveX? |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
Follow us on