12/17/2017 4:09 PM | |
Joined: 9/27/2006 Last visit: 9/25/2024 Posts: 12283 Rating: (2685) |
Translatiojn from the French:
Bonjour HH21; Cette section du forum de Siemens utilise l'anglais comme langue d'échange, car elle accueille des membres de nombreux pays; la plupart ne parlent pas français. Faites-nous la faveur d'écrire en anglais à votre prochaine visite. Hello HH21; This section of the Siemens forum uses English as an interchange language, since members here come from numerous countries where French is not spoken. Do us the favour of writing in English on your next visit. Hope this helps, Daniel Chartier Edit: In the Simatic world (S7-300, S7-400, S7-1500) you can connect to IEC 60870-5-101 serial protocol throuhgh different types of RTUs, based on Siplus RIC modules. Note that the IEC 60870 protocols, as well as DNP3 and IEC 61850 are mostly used in substation automation projects, which the Simatic products ae not usually interfaced with. Siemens Energy has a line of products and softwares (SICAM) for substation automation that you could have a look into, as an alternative: SICAM – Substation Automation - Industrial Automation For a presentation of the Simatic options for IEC RTUs, start by examining this brochure, and the extract attached below: For detailed info on Siplus RIC modules for different S7 CPUs, look at this link: http://w3.siemens.com/mcms/siplus/en/siplus-ric-telecontrol/pages/default.aspx Note that you can mount a Siplus RIC on ET 200S/ ET 200SP systems, but not on ET 200M. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 12/17/2017 6:50:45 PM |
|
Follow us on