2/23/2018 2:59 PM | |
Joined: 4/19/2013 Last visit: 4/2/2024 Posts: 61 Rating: (0) |
Hello friends, We had a PC OS crash. We repaired the OS. But after repairs when we try to open the WinCC project it is showing: 1. Configured Server is not available. Do you want to open the project using the local computer as the server. After clicking Start server locally after some times following message comes. 2. Cannot open WinCC project- Project Manager for configured WinCC Server is not already running - Start project manager for configured server. Also i am not able to open the SQL Server Management Studio. - it shows message Package 'Microsoft SQL Management Studio Package' failed to load. - Both warning and error and the application closes if I click Ok. Pictures attached for ref. Ref-WinCC7.0 SP3 Attachment1.pdf (233 Downloads) |
4/13/2018 9:25 AM | |
Joined: 6/19/2017 Last visit: 4/24/2024 Posts: 7959 Rating: (162) |
New question published by munir3444 is split to a separate thread with the subject When trying to start the .mcp application it says server not available. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on