10/27/2021 3:37 PM | |
Posts: 10 Rating: (1) |
I want to test one g120 x 160 KW drive with 4 kw motor to test my command circuit but when i input motor data in quick setting and run the motor nothing will happen,there is no error but the motor do not run? Is there a min motor power for 160 kw drive?is posible to run wh chane parameters? ------------------------------------------------------------------------------------------ |
Last edited by: CS Moderator at: 10/27/2021 17:39:41New subject after splitting |
|
10/28/2021 3:53 PM | |
Joined: 10/11/2006 Last visit: 4/26/2024 Posts: 5825 Rating: (789)
|
Hello, on page 20 of the Hardware Installation Manual of the PM240-2, you can find which motors are permissible. https://support.industry.siemens.com/cs/ww/en/view/109801104 E.g. for the 400 V Power Modules, induction motors are permissible in the range from 25 % … 150 % of the converter power. |
With best regards, |
|
This contribution was helpful to1 thankful Users |
Follow us on