5/4/2018 8:30 PM | |
Joined: 3/30/2011 Last visit: 9/18/2024 Posts: 736 Rating: (256) |
Hello, there are many micromaster models :MM420-MM30-MM440 this is the link for manuals MM440, please choose operating instruction for your inverter and search for "quick commissioning". If you have different model choose the right one. Hope this helps Best Regads |
Last edited by: mindware at: 5/4/2018 8:35:14 PM★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★ |
|
5/7/2018 10:20 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Hello, You need to provide more information like, MLFB number of drive, how you are trying to set parameters like is it with BOP or AOP etc. etc. Have you read the manual to understand the drive? If you would have studied it you would come to know the input supply specifications of drive. How it will work on 1phase supply? Please refer the attached sheet to set supply frequency. (Here I pressume your drive is MM440) HTH. AttachmentMM440 frequency setting.pdf (238 Downloads) |
5/7/2018 1:32 PM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Have tried factory reset? Set P010 = 10 donot apply any DI signals, set P0970=1 & check. HTH. |
5/7/2018 3:19 PM | |
Posts: 4 Rating: (0) |
I tried to set P0010 to that setting. However it will only be programmed to setting 0,1 or 30. Strange eh. NeilC |
Follow us on