5/13/2018 9:53 AM | |
Posts: 6 Rating: (0) |
[snip] I have another problem, though. I hope I'm in the right chat here. The IOT2000EDU CPU does not start after a power failure. The CPU stays on stop and I have to set the CPU to run via the TIA portal. In the TIA portal, I set Restart after power failure in the hardware configuration. Nevertheless, the CPU remains on STOP after a reboot of the IOT. How can I automatically set the CPU to run state? Translated with www.DeepL.com/Translator ------------------------------------------------------------------------------------------ |
Last edited by: IOT2000_Moderator at: 5/16/2018 9:21:01 AMNew subject after splitting Last edited by: Jen_Moderator at: 5/16/2018 12:50:49 PMDivision of questions into separate topics. |
|
5/18/2018 11:10 AM | |
Joined: 4/28/2015 Last visit: 9/9/2024 Posts: 3345 Rating: (379)
|
Hi, okay. Setting the PLC in autostart was the reason for the wrong location of the io.conf file, right? You can use the attached skript instead of your skript for the autostart. Then the PLC is started in the right context, the default location of the io.conf file is used AND the CPU is in run. Best regards! Attachmentiot2000edu_+set_run.zip (423 Downloads) |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
Follow us on