1/20/2016 10:38 AM | |
Joined: 1/21/2013 Last visit: 7/3/2024 Posts: 6 Rating: (0) |
I've a similar issue where i'm configuring a new ES (pcs7 v7.1) after all installations i found that there are no HMI application, HMI client & HMI Client ref etc in the hardware catalog. can any one see any reasons for the same. i've attached the screen shot of a normal ES with WinCC Hmi components in hardware cat. and one with out it. I'm in need of your suggestions and guidance in this respect as this is stopping me in configuring HMI Servers and clients. ------------------------------------------------------------------------------------------ AttachmentPCS7.rar (125 Downloads) |
Last edited by: VENKAT_VSM at: 1/20/2016 11:15:59 AMLast edited by: Min_Moderator at: 1/20/2016 3:19:27 PMNew subject after splitting |
|
3/21/2017 7:06 AM | |
Joined: 3/14/2008 Last visit: 9/17/2024 Posts: 2095 Rating: (936)
|
Have you tried to open the PCS7 example project which is installed automatically? Can you open the HMI object in there or is it also not visible. Also check out the following topic and see my post (third post). Maybe it is something with SQL. https://support.industry.siemens.com/tf/ww/en/posts/pcs7-v6-0-sp1-suddenly-all-wincc-application-disappeared/146677/?page=0&pageSize=10 |
Last edited by: Oreca at: 3/21/2017 7:19:22 AMIf I could help you, you can use the RATE button. Thank you. |
|
Follow us on