4/19/2016 12:34 PM | |
Joined: 1/27/2012 Last visit: 6/20/2024 Posts: 84 Rating: (1) |
Hello Do you mean port address required in netpro local connection or the physical port of CPU like port 1 and 2 in CPU PN-IO? I think it is port address in netpro. correct? ------------------------------------------------------------------------------------------ |
Last edited by: Blue Moderator at: 4/19/2016 1:04:58 PMNew subject after splitting |
|
4/19/2016 1:21 PM | |
Joined: 8/25/2006 Last visit: 9/18/2024 Posts: 2209 Rating: (278) |
Hello. Kaulquappe mean port numbers in the properties of connection in NetPro (look at screenshot). |
4/19/2016 1:29 PM | |
Joined: 11/21/2007 Last visit: 8/12/2024 Posts: 2325 Rating: (308)
|
The same Physical port can be configured for several different types on connections on different logical ports. |
There is no such thing as the last bug in a program |
|
This contribution was helpful to2 thankful Users |
Follow us on