6/10/2016 7:11 PM | |
Joined: 1/16/2012 Last visit: 9/8/2022 Posts: 72 Rating: (3) |
Hello, I'm trying to upload CPU 1214C DC/DC/DC. I create a new project with the unspecified CPU, detect its' configuration. Everything is fine. My IP is in the same subnet, but I don't think it's important. Then I try to compare Offline/online and the connection gets terminated. In HW config it shows that everything is incompatible. I tried to compile HW and go online again, but it gets terminated again. I can’t download, because it’s a running machine and I don’t want to mess it up. When I search for accessible devices, I can see that PLC and its’ blocks online, but I cannot copy them. I forgot to check whether the CPU model changes to CPUCommon. Any ideas what might be wrong? I’m using V13 SP1 and its’ FW is v4.1.1. I think it was created with V13 SP1 as well, but I’m not sure. Can it be the problem that it was downloaded with V13 and I’m trying to upload it with a newer version? Or was FW is v4.1.1 definitely downloaded with V13 SP1? Regards, Giedrius K.
------------------------------------------------------------------------------------------ |
Last edited by: Giedrius_Kai at: 6/10/2016 7:16:46 PMLast edited by: The Helping Hand at: 6/13/2016 10:31:21 AMNew subject after splitting |
|
This contribution was helpful to1 thankful Users |
4/26/2017 8:54 AM | |
Joined: 4/21/2017 Last visit: 9/20/2024 Posts: 21 Rating: (1) |
Hello Giedries_Kai. Did you solve the problem? I have the same issue with the exact CPU. Regards! |
11/23/2017 11:51 AM |
|
Posts: 50 Rating: (6) |
Check project lanquages |
Follow us on