6/14/2016 1:07 PM | |
Joined: 12/29/2011 Last visit: 1/1/2024 Posts: 20 Rating: (0) |
I am using a KTP700 and when I try to simulate my screen. I am using virtualbox as vm and i have to enable 3D acceleration. I can only see the desktop windows through the screen only. Shave mode. What is this? ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 6/14/2016 1:36:58 PMNew subject after splitting |
|
6/14/2016 1:30 PM | |
Joined: 6/3/2014 Last visit: 1/17/2023 Posts: 660 Rating: (191) |
Hello AlexSen, I guess he meant "Safe Mode"? http://blogs.vmware.com/kb/2010/02/how-to-boot-into-windows-safe-mode-in-your-vm.html |
~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ★ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ |
|
6/20/2016 12:25 PM | |
Joined: 5/12/2006 Last visit: 4/25/2024 Posts: 22228 Rating: (2980)
|
no Winodws Safe Mode needed to solve the prob! frióm the thread which solkve the problem: https://support.industry.siemens.com/tf/de/en/posts/141467/ now start the Install of the Guest Additions: 1.) Virtual Box Guest Additions 2.) Direct3D Support (experimental) If i install only the first one the issue always happen. Then i install it with the second box and say that i will use the WDDM Driver. And now after the Reboot the basic panel simulation works like the comfort, all datat displayed correctly. So try to install the additions again an select the experimental Direct3D and say that you will use the WDDM Drivers. Regards Christoph |
This contribution was helpful to1 thankful Users |
Follow us on