10/30/2015 8:29 PM | |
Posts: 1 Rating: (0) |
Hello,
I have a similar problem trying to transfer to a TP900 panel. I am using TIA11 tried to update the OS (firmware) and it did not fully go trough. I then rebooted the panel but now it only comes with a message that the operating system needs to be updated.
I try to connect thru USB or Ethernet and it is not working??
Do you guys know of any other way to update the OS??
Best Regards,
Ricardo D ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 10/31/2015 1:53:27 PMNew subject after splitting |
|
10/31/2015 3:38 PM | |
Joined: 3/28/2015 Last visit: 5/10/2024 Posts: 721 Rating: (213) |
Hello, Perhaps the following topics might help: 1-How do you do an "Operating system update" (OS update) or "Reset to factory settings" on operator panels?2-Which connector cables are available for connecting to SIMATIC Panels? |
Eng.Mohamed Ibrahim |
|
11/2/2015 11:17 AM | |
Joined: 8/3/2009 Last visit: 5/13/2024 Posts: 12933 Rating: (1646) |
HI in this FAQ is everything explained to transfer to the Panel over Ethernet. The same settings as to do an OS Update:
Bye Murof |
Last edited by: The Helping Hand at: 11/2/2015 4:31:53 PMMade the link clickable If this Information really helps, you could use the Rate function |
|
Follow us on