7/19/2018 3:47 PM | |
Posts: 1 Rating: (0) |
I'm fault finding on an old CNC lathe with an 820T controller. Control is reporting a fault with the KTK Mentor DC drive, but the drive says it's ok and open for business So I'd like to see what inputs on the PLC ladder actually trigger this 6006 error that the makers error text file translates as the KTK Spindle Drive error I've eventually got Siemens to let me download Step 7 and it's been expanding itself now for hours hopefully to install but it's taking hours which seem very odd - I'm not even sure it will do what I want The PLC program is attached as a TXT file I'd be very grateful if anyone can advise if STEP7 can indeed produce a view-able ladder from this file or how else I can do it AttachmentPLCPROG.txt (52 Downloads) |
Follow us on